Why am I seeing Unity Pro Error Message - R6025 - pure virtual function call?
This error dates back to Unity Pro v8.0. It was corrected in V8.0 using patches and no longer exists in current versions. If you are seeing it in a current version of Unity, it is likely that your project is running the V8.0 libset. If you export your project to ZEF/XEF and then open the file and build all, this will update the libset to the version of Unity that was used to export / import. Because this process forces us to build all offline, the processor will need to be stopped in order to transfer this new program to it.
Publicado para: Schneider Electric Mexico