¿Cómo podemos ayudarte hoy?

What is the lead length of an ETD500-NE-4 sensor?

Issue:
Lead length of an ETD500-NE-4 sensor.

Product Line:
HVAC / Field Devices

Environment:
Sensor

Cause:
Replacement / Installation / Maintenance

Resolution:
The sensor is 14" in length