¿Cómo podemos ayudarte hoy?

Is there an available replacement diaphragm for the V6600-04301 Robert Shaw valve ?

Issue:
Availability of diaphragm for old Robertshaw valve assembly.

Product Line:
HVAC / Field Devices

Environment:
Valves

Cause:
Replacement / Installation / Maintenance

Resolution:
There are no available replacement diaphragms for the Robertshaw assembly.
A new valve / actuator and linkage kit will need to be ordered . A VB-7313-0-4-02 valve with MK-4601 actuator and AV-401 linkage kit is suggested replacement .

Schneider Electric Mexico

Documentos adjuntos
V66 Robertshaw 3-Way Mixing Valve.pdf [433.14 KB]