What is the power consumption rating (watts) for the control voltage, of the ATS48?
Looking for the power consumption rating (watts) for the control voltage, of the ATS48?
Product Line:
Altistart 48
Environment:
All models and serial numbers
Cause:
Documentation
Resolution:
ATS48D17Y to ATS48C17Y- 30 W
ATS48C21Y to ATS48C32Y- 50 W
ATS48C41Y to ATS48M12Y- 80 W