¿Cómo podemos ayudarte hoy?

What is a cross for a Siebe valve MG862PKA used with a Bellimo actuator GM24MFT?

Issue:
Is there a Valve that can be used with a Bellimo actuator GM24-MFT?

Product Line:
Valves and Actuators

Environment:
Application

Cause:
Replacement

Resolution:
There is no Siebe Valve MG862PKA that could be found. From the description it sounds like you could use the VB-8303-0-5-12 valve which is a 2-1/2" 3-way Mixing/Diverting valve  and can be used with the Schneider Electric MS41-6343 Actuator.  The AV-609-1 linkage kit is used with the MS41-6343 Actuator as it can cause the AV-607-1 Linkage to bend.  An AV-609-1 Linkage, which has a thicker shaft, that won't bend, should be used. See attachment

Schneider Electric Mexico

Documentos adjuntos
VB-8303 F-27197-7.pdf [731.61 KB]
MS41-634X F-26745-7.pdf [1.17 MB]
AV-607-1 AV-609-1 Linkage F-27479-3.pdf [1.47 MB]