Issue:
Is there a replacement for the 3/4" VB-7263 series 2 Way valve ?
Product Line:
Valves and Actuators
Environment:
Application
Resolution:
The VB-7263-000-6-6 valve is obsolete with no equal replacement . This is due to the special O ring made for Humidification applications used by OEM Dri-teem Co.
The current VB-7263-0-4-06 valve can be used, with the O-ring material adequate for the Humidification application.
Is there a replacement for the 3/4" VB-7263 series 2 Way valve ?
Product Line:
Valves and Actuators
Environment:
Application
Resolution:
The VB-7263-000-6-6 valve is obsolete with no equal replacement . This is due to the special O ring made for Humidification applications used by OEM Dri-teem Co.
The current VB-7263-0-4-06 valve can be used, with the O-ring material adequate for the Humidification application.
Publicado para: Schneider Electric Mexico