Where do I find the Magelis HMIG5U2 OS Image?
Issue
Where do I find the Magelis HMIG5U2 (Windows Embedded Standard) OS Image?
Product Line
Magelis HMIGTU Series
Resolution
The Magelis HMIG5U2 OS Image can be found attached to this FAQ:
HMIG5U2 BIN Image file (7.3GB): HMIG5U2_V400_20190227.bin
-> This is attached as 8 separate 7-zip files ("HMIG5U2_V400_20190227.7z.001" through to "HMIG5U2_V400_20190227.7z.008"). You will need the 7-zip extraction tool from www.7-zip.org to extract the .BIN file.
Backup Recovery Tool v1.0.4.2 (3MB): BackupRecovery.exe
MD5 Hash (of the .exe): db3b62d9428c07decd06680cd4fada36
-> This is attached as "BackupRecovery_v1.0.4.2.zip" (a regular zip file that you can doubleclick on to open in Windows to extract it)
How to extract the .BIN file from the eight 7z files:
All the files are downloaded into the C:\HMIG5U2_v400\ folder here.
Open the folder in 7-zip, then double-click the HMIG5U2_V400_20190227.7z.001 file (green arrow):
That will reveal the .BIN file, where you can drag and drop it into a folder of your choice:
Note: This .BIN image file is not the same as for the older generation HMIG5U.