How to monitor RAM battery voltage onto Scadapack E devices?
Used Analog System Point 50061
This analog system point measures the available battery voltage. It is useful for measuring the operating environment of the RTU and returns a floating point value in the range 0...32.767 Vdc.
·Use the system point directly by assigning a point of this point number (50061) in the RTU database.
·Read the system point into a user-created SCADAPack Workbench or ISaGRAF 3 Workbench application as an integer or real variable from an input board connection.
Publicado para: Schneider Electric Mexico