¿Cómo podemos ayudarte hoy?

How can the ATV212 be programmed for forced local?

Issue:
ATV212 setup for forced local

Product Line:
Altivar 212

Environment:
All

Cause:
Might be using communications for monitoring but controlling by the drive's terminals

Resolution:
Forced local can be triggered by either of two ways:
  • Assigning F108 (always active logic) to 48, which keeps forced local active
  • Assigning F113 (RES terminal) to 48, which triggers forced local when RES is active