¿Cómo podemos ayudarte hoy?

What is the part number for the motor that goes into the AG13A020 actuator?

Issue:
Is there a replacement motor for the Erie Pop Top actuators ?

Product Line:
Valves and Actuators

Environment:
Maintenance

Cause:
Replacement

Resolution:
The replacement Motor is part number 30-158-A is the replacement 24VAC motor for the current AG13 actuators