What is the replacement Actuator for MP-481-729-0-2?
Issue:
Is there a cross for the MP-481-729-0-2 Actuator by Carrier ?
Product Line:
Valves and Actuators
Environment:
Maintenance
Cause:
Replacement
Resolution:
The MP-481-729-0-2 is an OEM ( Carrier) Actuator and can be ordered directly from them with part number 025-17175-002
Is there a cross for the MP-481-729-0-2 Actuator by Carrier ?
Product Line:
Valves and Actuators
Environment:
Maintenance
Cause:
Replacement
Resolution:
The MP-481-729-0-2 is an OEM ( Carrier) Actuator and can be ordered directly from them with part number 025-17175-002
Publicado para: Schneider Electric Mexico