Is there an SD Card Writer for the M580?
The M340 has an SD card writer utility available. Can this be used for the M580 SD cards?
Product line
Modicon M580
Resolution
No. As of July 16th, 2022, there is not an SD card writer that can be used for the M580 SD cards. The M340 Card Writer is not compatible with the M580 SD cards.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)