¿Cómo podemos ayudarte hoy?

Find how much memory size and available free memory in Scadapack E series devices.

To find how much memory is available and size using the following.
1. Connect to the Scadapack E RTU device using the Scadapack E configurator> Remote Command line.
On the command prompt type Free command.

2. using Putty and enable the telnet service or used the command line on the serial port of the Scadapack E series device.