¿Cómo podemos ayudarte hoy?

SESU tool returning DOWNLOAD_FAIL error 403

Issue
When attempting to download a SESU hot fix the following message is returned, "The remote server returned an error. (403) Forbidden."

Product line
Schneider Electric Software Update tool

Resolution
Typically this means that the firewall blocks the SESU downloads as they are raw executables. If the SESU server can not be added to trust list, you will need to manually download from either se.com or an FTP site which can be created for you if you open a tech support ticket requesting a specific hotfix.

Here is a link to the latest version of SESU (3.0.12) as any version lower than 2.5.0 will no longer function.
http://downloads.modicon.com/getFTPDoc.php/780ad1c88808c28cf740ff19bd659434
This link was last updated Jan 20th 2026