¿Cómo podemos ayudarte hoy?

How to configure identification information for the SCADAPack x70 device

To configure identification information for the SCADAPack x70 device

1.On the Configuration Tab, select SCADAPack > Settings.

2.Expand the Advanced Configuration parameters and configure the settings for:

The following table describes the Identification Strings parameters.
ParameterParameter Description
Location NameWhere the SCADAPack x70 device is installed.
Maximum length: 255 characters with spaces.
ID Code/NumberA numeric identifier for the SCADAPack x70 device.
Maximum length: 32 characters with spaces.
Device NameA name for the SCADAPack x70 device.
Maximum length: 32 characters with spaces.


3.Click Apply.