¿Cómo podemos ayudarte hoy?

What is the difference between the BMXFTB2010 and the BMXFTB2010TW?

Issue:
The terminal blocks seem the same but have different part numbers.

Product line:
X80 terminal blocks

Cause:
Part Number markings

Resolution:
There is no functional or technical difference between the BMXFTB2010 and the BMXFTB2010TW. Both products are identical in terms of features and specifications.

1. The only distinction is the "TW" suffix in the BMXFTB2010TW part number, which indicates that the product was manufactured in Taiwan.

2. The contents, performance, and application of both BMXFTB2010 and BMXFTB2010TW are the same.

Summary

You can use either the BMXFTB2010 or BMXFTB2010TW interchangeably, as the "TW" marking is solely for manufacturing origin identification and does not affect product compatibility or function.

Schneider Electric Mexico

Explora más
Producto:
Explora más
Producto: