¿Cómo podemos ayudarte hoy?

How to monitor the SCADAPack x70 time using Modbus.

  • Under the Configuration -SPx70 Controller in RemoteConnect select the object tab.
  • To add the Hour, Minutes and Seconds in the RemoteConnect Object.
  • In Object  Configuration, click add object and enter the following information below when monitoring the HOUR.
  • Assigning modbus register for the HOUR by selecting the modbus tab.
  • click add object and enter the following information below when monitoring the MINUTE.
  • Assigning modbus register for MINUTE by selecting the modbus tab.
  • click add object and enter the following information below when monitoring the SECOND.
  • Assigning modbus register for SECOND by selecting the modbus tab.
  • Hit Apply button then Write the program into the SCADAPackx70 to make changes.
  • Monitor the modbus registers assigned. In this example monitor register 40100 for HOUR, 40101 for MINUTE and 40102 for SECOND.