¿Cómo podemos ayudarte hoy?

How to determine if the SCADAPack x70 device will require the 5103 power supply module.

  • Launch the RemoteConnect software.
  • Create new program by selecting the correct controller type. In our Example the SCADAPack 474 was selected.
  • Under the Configuration tab>Physical IO>Local
  • Start adding all the IO requirements, You'll notice that the comment below the table stating the estimate power consumption and if a 5103 power supply module is required.
  • As you add more IO modules, an exclamation mark will appear on the table as a notification that it will require the 5103 power supply module.