¿Cómo podemos ayudarte hoy?

What is the short circuit current rating for the QO distribution panels?

Issue:
What is the short circuit current (SCCR)  rating for the QO distribution adaptors:   HQO206AB, HQO206BC, HQO206AC and HQO306

Product Line:
Panelboards

Environment:
I-Line circuit breaker panelboards and accessories

Resolution:
The adaptors themselves do not carry a short circuit current rating. They would have the short circuit current rating of the breakers used in them.