What is the depth of a QMB panel NEMA 1 box?
Dimensions of a QMB NEMA 1 enclosure
Product Line:
QMB Switchboards
Environment:
Switchboards and Switchgear
Resolution:
The standard depth of a NEMA 1 box for a QMB panel is 11.5 inches. If the panelboard is supplied with an optional trim with a door, the depth is 18 inches.