Are the SDSA1175 or SDSA3650 Secondary Surge Arrestors suitable for DC voltage?
Are the Secondary Surge Arrestors SDSA1175 or SDSA3650 usable on direct current systems?
Product Line:
Surge Arrestor
Environment:
SDSA1175 & SDSA3650 surge arrestors
Resolution:
These Secondary Surge Arrestors are rated for AC applications only