¿Cómo podemos ayudarte hoy?

I have a low voltage dry type distribution Transformer that has the number 79TS22C on the nameplate. Is this the catalog number?

Issue:
Markings on Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Transformer markings and NamePlates

Resolution:

No, this is a UL reference number which designates the manufacturing facity where the unit was built.

If the catalog number is not plainly apparent on the nameplate of the device, then a description of the transformer (voltage system in/out, kVA, temperature rise, conductor material, etc.) is required to identify a likely cross reference or updated style selection.