¿Cómo podemos ayudarte hoy?

What is the part number for the U-shaped Tinnerman clip used along with the screws to mount I-Line and larger vented hinged trim?

Issue:
What is the "U" or "C" shaped clip that is used in mounting panelboard trim pieces to the enclosure?

Product line:
Panelboards

Environment:
I-line, NQ, NF, QMB panelboards

Resolution:
The clip is a 1/4-20 Tinnerman clip, part number is 23301-02203.  LP9502 includes 8 of these clips and 8 matching screws.  Note that not all trims require Tinnerman clips.