¿Cómo podemos ayudarte hoy?

Needs to add lugs for a bigger wire size for 400SN Neutral Assembly

Issue:
Are optional lugs available for the 400SN neutral assembly?

Product Line:
Panelboards

Environment:
ILine Panelboards

Resolution:
Yes, optional lugs are available for the 400SN neutral assembly. The standard lug provided on the neutral assembly will accept (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil CU or AL conductors. Optional lugs include: AL400LH7 for (1) 350 -750 kcmil CU or AL conductor: CU400LA for (1) #1 AWG - 600 kcmil or (2) #1 AWG - 250 kcmil CU only conductors. The optional lug kits contain one lug. Two kits would be required to change both the incoming and outgoing neutral lugs.