¿Cómo podemos ayudarte hoy?

How deep are I-Line WP enclosures?

Issue:
Depth for I-Line Weatherproof enclosures

Product Line:
I-Line panelboards

Environment:
Products Sold in North America

Resolution:
26 inch wide WP`s for HCN interiors are 9.75 inches deep.
26 inch wide WP`s for HCP-SU interiors are 13.50 inches deep.
32 inch wide WP`s for HCM interiors are 11.75 inches deep.
42 inches wide WP`s for HCW, HCWM interiors are 12.95 inches deep.
44 inches wide WP`s for HCR-U interiors are 14.50 inches deep.