¿Cómo podemos ayudarte hoy?

Can a transformer for a 1 phase load work off a 3 phase power source?

Yes. A single-phase transformer can be fed from either a line-to-line or a line-to neutral source. Simply match the primary voltage rating of the transformer to the available source voltage.