¿Cómo podemos ayudarte hoy?

What are the repair parts for a QMB323TW Series E1 (E01)?

Issue:
QMB323TW Repair Parts

Product Line:
QMB

Environment
QMB Switch.

Cause:
Maintenance

Resolution:
The QMB323TW is a twin switch, meaning it contains two switches in the one device.  Parts are listed per switch.
Only the parts listed below are considered field replaceable:

Arc Shield/Suppressor Assembly (1 required) - 4051239950
Load Base Assembly (1 required, includes lugs) - 4052068050
Load Base Mounting Screw (2 required per load base) - 4020506501
Handle Knob Kit - 4028343750

Schneider Electric Mexico

Explora más
Rango:
Producto:
Explora más
Rango:
Producto: