¿Cómo podemos ayudarte hoy?

How many hold down/retainer kit spots are available in the top section of the Energy Center?

Issue:
Can more than one breaker be retained in the top section of the Energy Center?

Product Line:
Energy Center

Resolution:
A maximum of 10 clips can be used. 3 clips are already designated: 2 clips were factory included for the solar circuit breakers and 1 clip was factory assembled with the 110 A submain circuit breaker.