Does the power distribution block design of the Energy Center still have lug connections for connecting both top and bottom connections to the backup circuit?
Issue:
Does the power distribution block design of the Energy Center still have lug connections for connecting both top and bottom connections to the backup circuit?
Product Line:
Energy Center
Resolution:
The PDB has multiple lug connections per phase at its output. These are intended to allow either one or both submain breakers to be connected to power via an internal or external backup interface for grid isolation during backup mode. One breaker is connected this way from the factory to produce partial home backup. The other breaker can also be connected there to give whole house backup.
Does the power distribution block design of the Energy Center still have lug connections for connecting both top and bottom connections to the backup circuit?
Product Line:
Energy Center
Resolution:
The PDB has multiple lug connections per phase at its output. These are intended to allow either one or both submain breakers to be connected to power via an internal or external backup interface for grid isolation during backup mode. One breaker is connected this way from the factory to produce partial home backup. The other breaker can also be connected there to give whole house backup.
Publicado para: Schneider Electric Mexico