How does the Tru-Fault LED work on the new AF and AFGF circuit breakers?
What do the various flash patterns mean on the new Tru-Fault LED?
Product Line:
QO and HOM arc fault and dual function breakers
Resolution:
The LED light now included in the new AF and AFGF circuit breakers provides diagnosis through a visual indication of the trip event recorded.
When the circuit breaker trips, you can follow these options:
Use the troubleshooting guide included in your instruction bulletin.
Use the True-Fault LED to identify the last trip recorded.
Use the Time Saver Diagnostic (TSD) to identify the last trip report.
Note: if the LED light pulses 7 times, contact a certified electrician to replace the circuit breaker.