¿Cómo podemos ayudarte hoy?

How can you monitor the dc bus amps when you have a dc bus tie on two ATV930 Drives?

Issue:

Monitor the DC bus current with a DC bus tie on the ATV930 series drive.

Product Line:

Altivar ATV930 series only

Environment:

All

Cause:

Wants to read the dc amps when two drives are connected via DC bus.

Resolution:

You can't view the DC bus amps on the HMI so you would need to use a DC amp clamp on accessory for your meter.