¿Cómo podemos ayudarte hoy?

Are trip units for Powerpact H, J, and L circuit breakers replaceable?

Issue:
Can trip units for H, J, and L frame circuit breakers be replaced?

Product Line:
Circuit Breakers

Environment:
Powerpact H, J, L frames

Resolution:
Trip units for Powerpact H, J, and L can be replaced unless they have been sealed at the factory.
  • All I-Line breakers in this range have sealed trip units and are NOT replaceable.  I-Line breakers all have the letter "A" in the third position in the catalog number
    • for example, HJA36100U31X.
  • Unit mounted circuit breakers may be purchased with sealed or replaceable trip units
    • Breakers with replaceable trip units have a "T" in the catalog number immediately following the Ampere rating,
      • for example, HJA36100TU31X or HGA36100T
    • Breakers with sealed trip units will have no T in the catalog number in this position,
      • for example, HJA36100U31X or HGA36100
Check the current edition of the Square D Supplemental Digest or catalog numbers related to replaceable trip units.