¿Cómo podemos ayudarte hoy?

What is the minimum version of EcoStruxure Control Expert needed to configure the PMEPXM0100 Profibus module?

Issue:
Minimum version of  EcoStruxure Control Expert needed to configure the PMEPXM0100 Profibus module


Product Line:
Control Expert, PMEPMX0100


Resolution:
The minimum version of EcoStruxure Control Expert needed to configure the PMEPXM0100 Profibus module is V14.0 with the installation of hotfix ControlExpert_V140_HF_PMEPXM0100