¿Cómo podemos ayudarte hoy?

Control Expert V15.1 Security enforcement message

Issue

When creating a new project with Control Expert V15.1 the window shown below pops up.
234852_secenf

Product Line

Control Expert

Resolution

For cybersecurity reasons you will get the 'Security enforcement' window when initially creating a project. This is intended to make it very simple for the users requiring password protection in their projects. One can choose to create a password and hit OK or select Cancel and proceed without a password.