Where can I find ATV340 Control wiring diagram?
Issue:
Trying to locate ATV340 wiring terminations.
Product Line:
ATV340
Environment:
All
Cause:
Cannot find drawings
Resolution:
Control Block Wiring Diagram:

(1) 24V supply (STO)
(2) STO - Safe Torque Off
(3) PTI - Pulse Train In
(4) PTO - Pulse Train Out
(5) Motor Encoder connection
(6) Digital outputs
(7) Digital inputs
(8) Analog output
(9) Analog input
(10) Differential Analog Input
(11) Ethernet port (only on Ethernet drive version)
SW1 :Sink/Source switch
R1A, R1B, R1C :Fault relay
R2A, R2C :Sequence relay
Here is a link to the installation manual for additional wiring information.
https://www.se.com/us/en/download/document/NVE61069/
Publicado para: Schneider Electric Mexico