BMXSRA0405 relay contact material
Issue
Are the relays in the BMXSRA0405 gold plated and/or bifurcated?
Product line
M580 Safety
Resolution
The contacts are gold plated (NO 0,2 µm, NC 5 µm) and not bifurcated.
The relays are equipped with single crown contacts to ensure high switching
reliability.
Publicado para: Schneider Electric Mexico