Can you use the NQMB2Q on a 100A NQ panel?
Issue:
Needs an 18 circuit NQ panel with a 100A QD main breaker
Product Line:
Panelboards
Environment:
NQ Panelboard
Cause:
Field conversion
Resolution:
NQMB2Q main breaker kit will not work on an NQ 100A like the NQ18L1C
The 100A interior has main lugs rated for #6-2/0 AWG while the main breaker kit has cables rated for 4/0 AWG.
There is no way to make the connection between the breaker and the interior.
Publicado para: Schneider Electric Mexico