BMXNOE01x0 displaying a solid ERR
Issue
After configuring an NOE Ip address in the M340 project and properly linking it in the software and transferring, I see a solid ERR on the NOE module.
Product Line
Modicon M340, Control Expert, Unity Pro
Resolution
If the M340 and NOE Run are both on solid and the NOE still has a solid ERR light the most common cause is not cable.
No cable would be accompanied by ETH STS exhibiting 3 flashes.
See below the NOE indicator meanings.
Publicado para: Schneider Electric Mexico