ION 8650 Meter series firmware History
Issue
Customer may need to know about the old firmware or still have meters with old firmware.
Product Line
ION 8650 (A, B, and C variant)
ION 8600 obsolescence
Environment
Meter software – Firmware history
Cause
The customer my need to know the evolution and the change made on each firmware version for security purpose.
Resolution
The ION 8650 is our high utility device with variant A, B, and C. This replaced the ION 8600 obsolete in July 2011, since then the ION 8650 series meter has 15 firmware version from v400 to v004.040.001 as today.
The best way to search for firmware is the go: to Se.com -> Products -> Go to Download Center –> Enter your key word (ION 8650 firmware) you can find most of them, or from ION Setup software (Help -> ION Setup on Box -> ION Firmware -> then open ION 8650 folder. Also, please find attached an excel file with the firmware from version v400 to v004.040.001
Here, are some useful links related:
- ION Setup Page and Download Link
- ION8650 documentation: FA300091