¿Cómo podemos ayudarte hoy?

What are the replacement parts for transformer Enclosure Type 22M?

Product Line:

EX/EXN Transformer

Environment:

Low Voltage Transformer

Cause:

Replacement for the side panels (left and right) EXN150T3H enclosure.

Resolution:

Transformer Dry Enclosure Part 22M Base = PHA70314

Transformer Dry Enclosure Part 22M Front = PHA70315

Transformer Dry Enclosure Part 22M Rear = PHA70316

Transformer Dry Enclosure Part 22M Top = PHA79886

Transformer Dry Enclosure Part 22M Side = PHA70318

Note: To order the replacement front with the proper nameplate for the transformer, make sure to provide the following information Serial Number and Date code. A picture of the nameplate placed on the front panel and pictures of the coils labels is required to be included with the purchase order.

Schneider Electric Mexico

Explora más
Producto:
Explora más
Producto: