¿Cómo podemos ayudarte hoy?

140DAO84000 general information

Issue

1. Does this card have dry or wet contacts?

2. What would be the expected measurement on the channel? Some are reading at 22VAC to ground; some are reading at 115VAC.

3. The manual is not specific, is this module hot-swappable?

4. Where in programming software would you go to look for faults on this card?

Product Line
Modicon Quantum

Resolution
A1. The 140DAO84000 is a Triac output card, not a relay card with wet/dry contacts.

A2. This card has 16 isolated channels. Each channel could measure between 20 ... 253 VAC.

A3. Yes, this module is hot swappable.

A4. There is no access to the the individual channel indicators that appear on the module as below.

247883_img

But you can assign IO Map Status words to the racks in the drops and in this case a single bit will used from the byte assigned the respective slot from those words as below to indicate that at least a single channel has an issue.

247883_img1

Schneider Electric Mexico

Documentos adjuntos
140DAO84000.pdf [871.07 KB]
Explora más
Producto:
Explora más
Producto: