What programming software can be used for Modicon Micro?
The Modicon Micro controllers (110CPUxxxxx) were programmed using Modsoft (DOS) and ProWORX (Windows) obsolete software.
The most recent software that was used was ProWORX 32. The smallest package, ProWORX 32 Lite is all that was needed.
Neither software is currently available as an active sale but in the case of ProWORX 32, it is possible that the service team could provide it.
For pricing and availability regarding ProWORX 32 LITE, send an email to service.sales@se.com asking about part number 372SPU71001PLDV.
Publicado para: Schneider Electric Mexico