What is the maximum Control Expert Array Variable size?
The Array size limit remains/will remain at 64K.
Previous to CE v15.1 the array size of the DDT also could not exceed 64K bytes.
As of CE v15.1 the DDT maximum array size was increased to 2M bytes.
***The release notes of v15.1 implied that the array variable size was also increased but it was not. ***
Publicado para: Schneider Electric Mexico