¿Cómo podemos ayudarte hoy?

What is the Solid Neutral Assembly for use in the B125F, B125S, B125RB, B125DS, B125A, B125AWK Circuit Breaker Enclosures?

Issue:

Product design features

Product Line:

Circuit Breakers Enclosures

Environment:

Solid Neutral Assembly

Cause:

Application

Resolution:

The solid neutral assembly's used in these enclosures would be as follows:

1) For 15 - 100Amp breakers use solid neutral catalog number SN100FA

2) For 110 - 125Amp breakers use solid neutral catalog number SN225KA