¿Cómo podemos ayudarte hoy?

What is the replacement bottom plate for an EX transformer with a 25J type enclosure?

Product Line:

Low Voltage EX/EXN Transformer

Environment:

LV Transformer

Cause:

Looking for bottom plate for EX225T3H transformer that is mounted high up, i.e. billboard.

Resolution:

The EX225T3H has a 25J type enclosure. The 25J enclosure is designed to be "Switchboard Style", meaning it mimics our Switchboard Product's open-style bottom access for ease of conduit entry and wire bending, etc. As a result, the open bottom enclosure does not have an option for a bottom plate available at this time. We do not offer any bottom plate for Type 25J enclosure. Since the Transformer is normally placed on a concrete floor or pad, the customer may fabricate a shelf or metal barrier below the Transformer to prevent access to the underside, but any such installation is subject to the discretion of local inspection authorities.

Schneider Electric Mexico

Explora más
Producto:
Explora más
Producto: