What type of fuse does the PQ4610G plug-in unit accepts?
Product Line:
I-Line Busway fusible Plug-in unit
Environment:
I-Line Busway
Cause:
Trying to verify if PQ4610G will accept Class J fuse.
Resolution:
The PQ4610G takes Class H, K or R fuses. It also has provisions for Class J fuse. Provisions for installing Class J fuses are included in 30 A through 600 A fusible devices. Conversion to Class J fuse spacing requires relocating the load side fuse base assembly from standard Class H fuse location to an alternate position in the enclosure.
Publicado para: Schneider Electric Mexico