¿Cómo podemos ayudarte hoy?

Is the L shape bracket on SDSB80111 available on HEPD?

Issue:

What's the installation bracket for HEPD80/50?

Product Line:

Surge Protection Devices

Answer:

The bracket is only available on the SDSB and not for HEPD. There's no bracket for the HEPD. Only available mounting kit is the flush mounting kit HEPD58MKF.