What is the inrush for an EX150T3HCUNLP?
Issue:
Inrush for EX150T3HCUNLP
Product Line:
Low voltage Transformer
Environment:
Products sold in North America
Resolution:
The inrush of an EX150T3HCUNLP is 7.6 times the Full Load Amperage (FLA) of the Primary. The Primary FLA (at 480V) is 180A. 180A x 7.6 = an Inrush of 1,368A.
Publicado para: Schneider Electric Mexico