Can you order the outer door lock separately and install in the field?
Product Line:
Panelboard
Environment:
RTI Panelboard
Cause:
Need to convert NC74SHR to NC74SHRODL.
Resolution:
NO, the outer door locks (ODL) are not available RTI and are not field installable. Covers with "ODL" suffix has another lock added to the outer left edge of the mat to lock the entire trim against the box flange.
Publicado para: Schneider Electric Mexico