I-Line Panelboard Phasing
Product Line:
I-Line Panelboard
Environment:
Low Voltage Panelboard
Cause:
Verification on phase arrangement on the bus stack of an I-Line panelboard, front to back.
Resolution:
All I-line three pole breakers are standard ABC. When they are installed on the Left side of the bus, top to bottom is ABC. When they are put on the right side of the bus, they are CBA top to bottom. This is standard unless when quoted, the Structure option is selected to have the right side of the bus be ABC.
Publicado para: Schneider Electric Mexico